Switchbot and Wio Terminal

Hi! Thank you.
I get the same:

11:21:12.715 -> BATT Device found: Name: , Address: 30:32:90:2e:39:c8
11:21:12.750 -> new BLEAdvertisedDevice
11:21:12.750 -> new BLEAdvertisedDevice done
11:21:12.750 -> Forming a connection to 30:32:90:2e:39:c8
11:21:12.750 -> - Created client
11:21:12.820 -> BLE Advertised Device found: Name: , Address: 18:4b:8a:df:90:60
11:21:12.890 -> BLE Advertised Device found: Name: , Address: 0b:1c:86:86:8c:59, serviceUUID:
11:21:15.085 -> - Connected to server
11:21:19.654 -> ScanCallback: GAP_MSG_LE_CONN_UPDATE_IND: conn_id 0, conn_interval_max 0x18, conn_interval_min 0x6, conn_latency 0x0,supervision_timeout 0x190
11:21:19.654 ->
cba20d00-224d-11e6-9fb8-0002a5d5c51b
11:21:30.151 -> Failed to find our service UUID: cba20d00-224d-11e6-9fb8-0002a5d5c51b
11:21:30.185 -> We have failed to connect to the server; there is nothin more we will do.
11:21:30.185 -> …