Support for the Seeed Round Display?

Hi there,
SO, Super Citric Fly’s in and Saves the DAY… NICE one :+1: Working Good Here.!

Here is my successful code demo and it works for both the C3 or C6 without edit.
I loaded some older code too and it worked without using the older TFT_eSPI lib, ver 2.5.23
Very Good!
I have not tested it in conjunction with WiFi or BLE I’ll try that next.
" this is a gauge demo with a Pointer value in the center (after the scrolling text)"
Compiler output and Serial output bellow. :face_with_monocle:


New ROLex…

Gauge Demo

//This will make the meter visually alert you when the reading crosses 45, with both the gauge and the displayed number turning red.
//
// TFT_eSPI.h Version [email protected], updated from https://github.com/Seeed-Projects/SeeedStudio_TFT_eSPI
// BSP is 3.0.5 
// Xiao ESP32C6 AOK :-)
// tested  10/14/24 by PJ Glasso
//
#include <SPI.h>
#include <TFT_eSPI.h>

TFT_eSPI tft = TFT_eSPI(); 

#define WHITE       0xFFFF
#define BLACK       0x0000
#define BLUE        0x001F
#define RED         0xF800
#define GREEN       0x07E0
#define YELLOW      0xFFE0
#define GREY        0x2108
#define TEXT_COLOR  0xFFFF
#define SCALE0      0xC655
#define SCALE1      0x5DEE

#define DEG2RAD     0.0174532925

int xpos = 0;
int ypos = 0;
int gap = 55;
int radius = 120;
int angle;
uint32_t runTime = -99999;
int reading;
int d = 0;
bool range_error = 0;
float rt_x, rt_y, rl_x, rl_y, rr_x, rr_y;
float rt_x_old, rt_y_old, rl_x_old, rl_y_old, rr_x_old, rr_y_old;
float angle_top,  angle_rechts, angle_links;
float center_x = 120;
float center_y = 125;
float temp_00; 
uint32_t chipId = 0;

void setup(void) {
  tft.begin();
  Serial.begin(9600);
  delay (2000);
  Serial.println( "Starting UP , Round Display Test...");
      Serial.println();
   for(int i=0; i<17; i=i+8) {
	  chipId |= ((ESP.getEfuseMac() >> (40 - i)) & 0xff) << i;
	  }
  Serial.printf("ESP32 Chip model = %s Rev %d\n", ESP.getChipModel(), ESP.getChipRevision());
	Serial.printf("This chip has %d cores\n", ESP.getChipCores());
  Serial.print("Chip ID: "); Serial.println(chipId);

  tft.setRotation(0);
  tft.fillScreen(BLACK);

  // Scroll "PJ_Seeed" message in the center for 20 seconds
  scrollText("PJ_Seeed", BLUE, 10 * 1000);  // Display for 20 seconds
  tft.fillScreen(BLACK);   // Clear the screen
}

void loop() {
  if (millis() - runTime >= 0L) {
    runTime = millis();

    temp_00 = random(00, 100); // Simulate random value for testing
    reading = temp_00;
    
    indexTag();  // Update the index tag

    if (reading > 45) {
      ringMeter(reading, 0, 100, xpos, ypos, radius, RED);  // Red gauge if reading > 90
      drawText(String(reading), 120, 125, RED);             // Red font if reading > 90
    } else {
      ringMeter(reading, 0, 100, xpos, ypos, radius, GREEN); // Green gauge for normal range
      drawText(String(reading), 120, 125, WHITE);            // White font for normal range
    }

    delay(1000);  // Wait before next update
  }
}

// Function to scroll text across the screen
void scrollText(String text, uint16_t color, uint32_t duration) {
  uint32_t startTime = millis();
  int textWidth = tft.textWidth(text);
  int xStart = tft.width();  // Start the text off the screen (right side)
  int xEnd = -textWidth;     // End when the text is completely off the screen (left side)

  while (millis() - startTime < duration) {
    int xPos = map(millis() - startTime, 0, duration, xStart, xEnd);
    tft.fillScreen(BLACK);   // Clear the screen
    tft.setTextColor(color, BLACK);
    tft.setTextSize(2);      // Adjust text size as needed
    tft.setCursor(xPos, tft.height() / 2 - 10);  // Center the text vertically
    tft.print(text);
    delay(250);               // Control the scroll speed
  }
}


void drawText(String value, int x, int y, uint16_t color) {
  // Clear a large enough area where the previous text was displayed (with background color)
  int16_t textWidth = tft.textWidth("000");   // Estimate the maximum width for a 3-digit number
  int16_t textHeight = 24;  // Adjust based on text size

  // Fill the area with the background color (BLACK) to ensure old digits are cleared
  tft.fillRect(x - (textWidth / 2), y, textWidth, textHeight, BLACK);

  // Set the new text color and print the new value
  tft.setTextColor(color, BLACK);  // Set text color with background as BLACK
  tft.setTextSize(3);              // Adjust text size as needed
  tft.setCursor(x - (tft.textWidth(value) / 2), y);  // Center the text
  tft.print(value);  // Display the new value
}

// Draw the meter on the screen
int ringMeter(int value, int vmin, int vmax, int x, int y, int r, uint16_t scheme) {
  x += r;
  y += r;
  int w = r / 3;
  angle = 150; 
  int v = map(value, vmin, vmax, -angle, angle);
  byte seg = 3;
  byte inc = 6;

  for (int i = -angle + inc / 2; i < angle - inc / 2; i += inc) {
    float sx = cos((i - 90) * DEG2RAD);
    float sy = sin((i - 90) * DEG2RAD);
    uint16_t x0 = sx * (r - w) + x;
    uint16_t y0 = sy * (r - w) + y;
    uint16_t x1 = sx * r + x;
    uint16_t y1 = sy * r + y;
    float sx2 = cos((i + seg - 90) * DEG2RAD);
    float sy2 = sin((i + seg - 90) * DEG2RAD);
    int x2 = sx2 * (r - w) + x;
    int y2 = sy2 * (r - w) + y;
    int x3 = sx2 * r + x;
    int y3 = sy2 * r + y;

    if (i < v) {
      tft.fillTriangle(x0, y0, x1, y1, x2, y2, scheme);
      tft.fillTriangle(x1, y1, x2, y2, x3, y3, scheme);
    } else {
      tft.fillTriangle(x0, y0, x1, y1, x2, y2, GREY);
      tft.fillTriangle(x1, y1, x2, y2, x3, y3, GREY);
    }
  }
  return x + r;
}

// Draw the index tag
void indexTag() {
  tft.fillTriangle(rt_x_old, rt_y_old, rl_x_old, rl_y_old, rr_x_old, rr_y_old, BLACK);
  
  angle_top = -(240 * DEG2RAD) + ((3 * temp_00) * DEG2RAD);
  angle_links  = (angle_top - (6 * DEG2RAD));
  angle_rechts = (angle_top + (6 * DEG2RAD));
  
  rt_x = (center_x + ((radius - 45) * cos(angle_top)));
  rt_y = (center_y + ((radius - 45) * sin(angle_top)));

  rl_x = (center_x + ((radius - 60) * cos(angle_links)));
  rl_y = (center_y + ((radius - 60) * sin(angle_links))); 
  
  rr_x = (center_x + ((radius - 60) * cos(angle_rechts)));
  rr_y = (center_y + ((radius - 60) * sin(angle_rechts))); 

  rt_x_old = rt_x;
  rt_y_old = rt_y;

  rl_x_old = rl_x;
  rl_y_old = rl_y;
  
  rr_x_old = rr_x;
  rr_y_old = rr_y;

  tft.fillTriangle(rt_x, rt_y, rl_x, rl_y, rr_x, rr_y, YELLOW);   
}

Compiler output that counts…

FQBN: esp32:esp32:XIAO_ESP32C6
Using board 'XIAO_ESP32C6' from platform in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\esp32\hardware\esp32\3.0.5
Using core 'esp32' from platform in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\esp32\hardware\esp32\3.0.5
EDIT--- For ___Brevity...
Using library SPI at version 3.0.5 in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\esp32\hardware\esp32\3.0.5\libraries\SPI 
Using library TFT_eSPI at version 2.5.43 in folder: D:\Arduino_projects\libraries\TFT_eSPI 
Using library FS at version 3.0.5 in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\esp32\hardware\esp32\3.0.5\libraries\FS 
Using library SPIFFS at version 3.0.5 in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\esp32\hardware\esp32\3.0.5\libraries\SPIFFS 
"C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\esp32\\tools\\esp-rv32\\2302/bin/riscv32-esp-elf-size" -A "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\02E327668A7C72E8CA85338770FE5BA0/sketch_oct14a_scroll_pjg_C6_round_eye.ino.elf"
Sketch uses 272642 bytes (20%) of program storage space. Maximum is 1310720 bytes.
Global variables use 13208 bytes (4%) of dynamic memory, leaving 314472 bytes for local variables. Maximum is 327680 bytes.

Serial output…

Starting UP , Round Display Test...

ESP32 Chip model = ESP32-C6 Rev 1
This chip has 1 cores
Chip ID: 16776721

HTH
GL :slight_smile: PJ :v: