STM32F030K6T6 Pa7 Question

Hi everyone,

Nowadays, I am working on STM32F030K6T6 with mikroc for the arm. I have a question which is about this microcontroller.

when I use pa7 pin digital like this GPIO_Digital_Output(&GPIOA_BASE, _GPIO_PINMASK_7); after programming, I can’t reach the microcontroller in a normal way. when I want to program MCU, respectively, I have to push the reset pin, click the program icon, and then pull my hand on the reset pin.

As you can see, I am not using SWD pins but I am having a problem like SWD pins problem. I had been looking at stm32f030k6t6’s datasheet and I didn’t know anything about this issue.

Is there anyone who coped up with this problem?

C46830_STM32F030K6T6_2015-04-27.PDF.zip (796.5 KB)