The specs, schematics and descriptions for the stalker v2.2 in the wiki are just copy-pasted from the v2.1 page. Where can I find the schematics for the v2.2?
Specifically, I have the following questions:
-
The v2.1 has two sets of i2c headers, one for 3.3V logic and one for 5V. The 2.2 has a single set of header, for which vcc is connected to Vin of the kb33 regulator next to the arduino reset pin, but you write that voltage is selectable. HOW?
-
What happend to CH_READ, OK_READ and BATT_READ? The jumpers don’t exist anymore. are the the traces still there? can I read the battery voltage on adc7 and charge and ok on pins 6 and 7? There seems to be something connected to ADC6, but I don’t understand how the status can be read

-
Is there a specific reason why D7 and D8 are broken out separately between the ftdi and i2c headers?
Please answer quickly, I’m kinda stuck.
Thanks!
Till