EdK
1
MY FIRST POST
I just received and tested the Grove Speech Recognizer but the two output lines seem to be always high when using an led as a logic probe.
The Arduino is not recognizing the outputs from the speech module.
Should the two output lines appear high all the time? What should I see at the outputs while resting and issuing a command?
Ed
Baozhu
2
This module uses serial port for communication, which cannot be used by simply checking the level.
For details, see the product Wiki documentation.
https://wiki.seeedstudio.com/Grove-Speech_Recognizer/
EdK
3
Thanks!
I imaging hooking it up to a pc serial port using a terminal program set correctly using TX, RX, and GND would show the output for testing.
Ed