Spartan Edge constraints file ? (or golden top etc)

Hi,
Is there a golden top level, a reference design or a pin assignment file available somewhere ?
It is tedious and error prone to parse the schematics and rebuild this.
It is typically provided with all commercial boards, like a BSP for processor boards.
Thanks in advance,
Bert

Bert : you are lazy… Do it !

Okay…
I wrote the proper XDC (not all signals though, just the ones from the devices on-board).
Just tested HDMI + LEDs + RGB LEDs (equivalent to WS2812 apparently).
I still need to understand how to use the on-board Flash for easier FPGA configuration.
It should be possible without involving the ESP32 (hopefully).