Hi there,
Thank you Josie…
ESP32-S31 vs. ESP32-S3: Should the XIAO Get an Upgrade?
By Josie Last Updated on: June 25, 2026
ESP32-S31 deep dive: Comparing with ESP32-S3. Should the next XIAO use this chip? what do you
think.
Best BLOG ever on the topic.
I’ll bring the Low Lights , just to keep it a ![]()
but Go READ it if you are serious about technology and the Paths up ahead, ![]()
Here are some LOW lights first from her Blog to keep it in perspective, as to why diving in headfirst isn’t always a good business decision. IMO.. BRAVO, Josie on the most excellent writing.
What the Community Is Actually Worried About
That all sounds impressive on paper. But here’s what developers are actually asking:
It’s RISC-V, not Xtensa. The ESP32-S series has always used Tensilica cores. Switching architectures raises real questions about toolchain maturity, existing library compatibility, and migration effort.
Arduino support is not ready. There’s an open GitHub issue requesting ESP32-S31 support in the Arduino core — it’s not merged yet.
You can’t buy it yet. Espressif confirms only “select customers” have received samples. No public pricing. No release date. If you need to build something today, this is a blocker.
Seeed needs more info like this in the public forums too… :
:
https://www.seeedstudio.com/blog/2026/04/14/esp32-s31-vs-esp32-s3-should-the-xiao-get-an-upgrade/
HTH
AS You were…
GL
PJ ![]()