Serial camera

I bought this:
seeedstudio.com/depot/grove- … p-945.html

Hooked up serial TX,RX, 5v, Gnd. When I power it on I see on PC terminal:
.Ctrl infr exist
.User-defined sensor
.625
.Init end

But it does not respond to any commands. That means I hooked up the 4 wires correctly, not backwards. That means I have the correct baud rate. I tried sending:
0x56 0x00 0x26 0x00
and
0x56 0x00 0x36 0x01 0x00
nothing in response. Not the above text, Assembled a packet in X-CTU.

What can I test next? Please help!

Tried loopback test with wire to make sure UART is working.

If you think you can help me please join this discussion:
arduino.cc/forum/index.php/topic,92367.0.html