SenseCAP T1000a no longer connects to TTN

Hi Jovelyn,

Thanks for your email; hereby my answers to your questions:

  • Firmware: 2.8

  • Notification rules: Only one rule (>10%)

  • Compare the timestamps: As you can see in the screenshots, there are no delayed or cached events

  • Connectivity issues: The LoRaWAN coverage is not very stable in the center of Amsterdam, but I did not press the SOS button that many times (I can see more than 20 notifications in the last 24 hours)

The notifications appear with a small delay after a data update.

I have the device for testing purposes — I only have one device and one user account.

I don’t see the GNSS Data Cache working at all, even though I have it enabled.

Kind regards

mattijs