Hi Everyone!
Does anyone know what are the usable voltages for the T1000-E’s TCXO? Is that some kind of standard module with 1.6-3.3V? I can’t seem to find the model used or any other parameter.
Thanks!
The SenseCAP T1000-E Card Tracker’s documentation does not specify the exact TCXO (Temperature Compensated Crystal Oscillator) model or its operating voltage.
yep, I know, I’ve searched everywhere, hoped that somebody can help me here ![]()
Hi there,
So the schematic is NOT open source AFAIK so , the devices Operating Temp range may give a clue. -20 t0 +60c
is all you get really at this point. What is your goal ?
HTH
GL
PJ ![]()
you might look at the Lora dev board schematic, that may give you the info also. Semitech stuff is very closed. BTW ![]()
My goal is to know the exact control voltages I can use for the TCXO.
Something like this (this is from another tcxo’s datasheet):
TCXO_CTRL_1_6V = 0x00
TCXO_CTRL_1_7V = 0x01
TCXO_CTRL_1_8V = 0x02
TCXO_CTRL_2_2V = 0x03
TCXO_CTRL_2_4V = 0x04
TCXO_CTRL_2_7V = 0x05
TCXO_CTRL_3_0V = 0x06
TCXO_CTRL_3_3V = 0x07
I’ve seen 1.6 or 1.8v in most usages for these. The ranges you posted look like what the LR1110 can be programmed with. I suspect anything between 1.6 and about 3.1 would work (I’ve seen another chipset say to use 200mV lower than supply, which is 3.3V for most of these.)