Hi there,
So got it working here…I’m not using the SD card btw… wiring is a bit SKetch but hay it’s late.
![]()
Runs on Battery too!
A couple observations, I using an Xiao Nrf52840 Sense UPLOADING the Xiao must be in bootloader mode with drive present.
I’m using the Crystalfontz.com LIB Worked right away.
#include <epd4in2.h>
#include <epdif.h>
#include <epdpaint.h>
#include <fonts.h>
#include <imagedata.h>
//=============================================================================
// "Arduino" example program for Crystalfontz ePaper.
//
// This project is for the CFAP122250A2-0213 :
//
// https://www.crystalfontz.com/product/CFAP122250A2-0213
//
// It was written against a Seeduino v4.2 @3.3v. An Arduino UNO modified to
// operate at 3.3v should also work.
//-----------------------------------------------------------------------------
// This is free and unencumbered software released into the public domain.
//
// Anyone is free to copy, modify, publish, use, compile, sell, or
// distribute this software, either in source code form or as a compiled
// binary, for any purpose, commercial or non-commercial, and by any
// means.
//
// In jurisdictions that recognize copyright laws, the author or authors
// of this software dedicate any and all copyright interest in the
// software to the public domain. We make this dedication for the benefit
// of the public at large and to the detriment of our heirs and
// successors. We intend this dedication to be an overt act of
// relinquishment in perpetuity of all present and future rights to this
// software under copyright law.
//
// THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND,
// EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF
// MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT.
// IN NO EVENT SHALL THE AUTHORS BE LIABLE FOR ANY CLAIM, DAMAGES OR
// OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE,
// ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR
// OTHER DEALINGS IN THE SOFTWARE.
//
// For more information, please refer to <http://unlicense.org/>
//=============================================================================
// Connecting the Arduino to the display
//
// ARDUINO |Adapter |Wire Color |Function
// --------+--------+-----------+--------------------
// D3 |17 |Green |Busy Line
// D4 |18 |Brown |Reset Line
// D5 |15 |Purple |Data/Command Line
// D10 |16 |Blue |Chip Select Line
// D11 |14 |White |MOSI
// D13 |13 |Orange |Clock
// 3.3V |5 |Red |Power
// GND |3 |Black |Ground
//
// Short the following pins on the adapter board:
// BS2 -> GND
// RESE -> 2.2ohms
//=============================================================================
//Connecting the Arduino to the SD card
//A CFA10112 micro SD card adapter can be used: https://www.crystalfontz.com/product/cfa10112
//
// ARDUINO |Wire Color |Function
// ---------+-----------+--------------------
// D8 |Blue |CS
// D11 |Green |MOSI
// D12 |Purple |MISO
// D13 |Brown |CLK
//
//
//=============================================================================
// Creating image data arrays
//
// Bmp_to_epaper is code that will aid in creating bitmaps necessary from .bmp files.
// The code can be downloaded from the Crystalfontz website: https://www.Crystalfontz.com
// or it can be downloaded from github: https://github.com/crystalfontz/bmp_to_epaper
//=============================================================================
// The display is SPI, include the library header.
#include <SPI.h>
#include <SD.h>
//#include <avr/io.h>
// Include the images. These images were prepared with "bmp_to_epaper" which
// is available on the Crystalfontz site.
#include "Images_for_CFAP122250A20213.h"
#define ePaper_RST_0 (digitalWrite(EPD_RESET, LOW))
#define ePaper_RST_1 (digitalWrite(EPD_RESET, HIGH))
#define ePaper_CS_0 (digitalWrite(EPD_CS, LOW))
#define ePaper_CS_1 (digitalWrite(EPD_CS, HIGH))
#define ePaper_DC_0 (digitalWrite(EPD_DC, LOW))
#define ePaper_DC_1 (digitalWrite(EPD_DC, HIGH))
#define EPD_BUSY 3
#define EPD_RESET 4
#define EPD_DC 5
#define EPD_CS 10
#define SD_CS 8
#define VRES 300
#define HRES 400
#define WAIT_BUSY while (0 != digitalRead(EPD_BUSY))
//=============================================================================
//this function will take in a byte and send it to the display with the
//command bit low for command transmission
void writeCMD(uint8_t command)
{
ePaper_DC_0;
ePaper_CS_0;
SPI.transfer(command);
ePaper_CS_1;
}
//this function will take in a byte and send it to the display with the
//command bit high for data transmission
void writeData(uint8_t data)
{
ePaper_DC_1;
ePaper_CS_0;
SPI.transfer(data);
ePaper_CS_1;
}
//===========================================================================
void fullUpdate(void)
{
//
writeCMD(0x22);
writeData(0xf7);
writeCMD(0x20);
}
void partialUpdate(void)
{
//
writeCMD(0x22);
writeData(0xff);
writeCMD(0x20);
}
//===========================================================================
void setup(void)
{
//Debug port / Arduino Serial Monitor (optional)
Serial.begin(9600);
delay (1000);
Serial.println("setup started");
// Configure the pin directions
pinMode(EPD_CS, OUTPUT);
pinMode(EPD_RESET, OUTPUT);
pinMode(EPD_DC, OUTPUT);
pinMode(EPD_BUSY, INPUT);
pinMode(SD_CS, OUTPUT);
digitalWrite(SD_CS, LOW);
if (!SD.begin(SD_CS))
{
Serial.println("SD could not initialize");
}
//Set up SPI interface
SPI.beginTransaction(SPISettings(2000000, MSBFIRST, SPI_MODE0));
SPI.begin();
initEPD();
Serial.println("setup complete");
}
//================================================================================
void initEPD()
{
//-----------------------------------------------------------------------------
//more detail on the following commands and additional commands not used here
//can be found on the CFAP176264A0-0270 datasheet on the Crystalfontz website
//-----------------------------------------------------------------------------
//reset driver
ePaper_RST_0;
delay(40);
ePaper_RST_1;
delay(40);
//Software Reset
WAIT_BUSY;
writeCMD(0x12);
WAIT_BUSY;
//Get out of deep sleep if we're there already
writeCMD(0x10);
writeData(0x00);
//Driver Output Control
writeCMD(0x01);
writeData(0xf9);
writeData(0x00);
writeData(0x00);
//Data Entry mode setting
writeCMD(0x11);
writeData(0x01);
//Set RAM X - address Start / End position
writeCMD(0x44);
writeData(0x00);
writeData(0x0F);
//Set RAM Y - address Start / End position
writeCMD(0x45);
writeData(0xF9);
writeData(0x00);
writeData(0x00);
writeData(0x00);
//Border Waveform Control
writeCMD(0x3C);
writeData(0x05);
//Display Update Control 1
writeCMD(0x21);
writeData(0x00);
writeData(0x80);
//Temperature Sensor Control
writeCMD(0x18);
writeData(0x80);
// Set RAM X and RAM Y address counter
writeCMD(0x4E);
writeData(0x00);
writeCMD(0x4F);
writeData(0xF9);
writeData(0x00);
WAIT_BUSY;
}
//================================================================================
void partialUpdateSolid(uint8_t x1, uint8_t y1, uint16_t x2, uint16_t y2, uint8_t color)
{
//Border Waveform Control
writeCMD(0x3C);
writeData(0x80);
//Set RAM X - address Start / End position
writeCMD(0x44);
writeData(x1);
writeData(x2);
//Set RAM Y - address Start / End position
writeCMD(0x45);
writeData(y1 & 0xff);
writeData(y1 >> 8);
writeData(y2 & 0xff);
writeData(y2 >> 8);
// Set RAM X and RAM Y address counter
writeCMD(0x4E);
writeData(x1);
writeCMD(0x4F);
writeData(y1 & 0xff);
writeData(y1 >> 8);
writeCMD(0x24);
int i;
int h;
for (h = 0; h < y2 - y1; h++)
{
for (i = 0; i < (x2 - x1) / 8; i++)
{
writeData(color);
}
}
//partial refresh of the same area as the partial update
partialUpdate();
WAIT_BUSY;
initEPD();
}
//================================================================================
void setBaseMap(const uint8_t *holder)
{
writeCMD(0x24); //Write Black and White image to RAM
for (int i = 0; i < MONO_ARRAY_SIZE; i++)
{
writeData(pgm_read_byte(&holder[i]));
}
writeCMD(0x26); //Write Black and White image to RAM
for (int i = 0; i < MONO_ARRAY_SIZE; i++)
{
writeData(pgm_read_byte(&holder[i]));
}
fullUpdate();
}
//================================================================================
void partialUpdateCharacters(const uint8_t *holder)
{
//x1 must be divisible by 8
uint16_t x1 = 0;
uint16_t y1 = 100;
uint16_t x2 = x1 + (64 / 8) - 1;
uint16_t y2 = y1 + (58) - 1;
//reset driver
ePaper_RST_0;
delay(40);
ePaper_RST_1;
delay(40);
//Border Waveform Control
writeCMD(0x3C);
writeData(0x80);
//Set RAM X - address Start / End position
writeCMD(0x44);
writeData(x1);
writeData(x2);
//Set RAM Y - address Start / End position
writeCMD(0x45);
writeData(y1 & 0xff);
writeData(y1 >> 8);
writeData(y2 & 0xff);
writeData(y2 >> 8);
// Set RAM X and RAM Y address counter
writeCMD(0x4E);
writeData(x1);
writeCMD(0x4F);
writeData(y1 & 0xff);
writeData(y1 >> 8);
writeCMD(0x24);
int i;
int h;
for (h = 0; h <= y2 - y1; h++)
{
for (i = 0; i < (x2 - x1 + 1); i++)
{
writeData(~pgm_read_byte(&holder[i + h * 8]));
}
}
//partial refresh of the same area as the partial update
partialUpdate();
WAIT_BUSY;
}
//================================================================================
void show_BMPs_in_root(void)
{
File
root_dir;
root_dir = SD.open("/");
if (0 == root_dir)
{
Serial.println("show_BMPs_in_root: Can't open \"root\"");
return;
}
File
bmp_file;
while (1)
{
bmp_file = root_dir.openNextFile();
Serial.println(bmp_file);
if (0 == bmp_file)
{
// no more files, break out of while()
// root_dir will be closed below.
break;
}
//Skip directories (what about volume name?)
if (0 == bmp_file.isDirectory())
{
//The file name must include ".BMP"
if (0 != strstr(bmp_file.name(), ".BMP"))
{
Serial.println(bmp_file.name());
//The BMP must be exactly 36918 long
//(this is correct for182x96, 24-bit)
uint32_t size = bmp_file.size();
Serial.println(size);
if ((uint32_t)HRES * VRES * 3 + 50 <= size <= (uint32_t)HRES * VRES * 3 + 60)
{
Serial.println("in final loop");
//Make sure the display is not busy before starting a new command.
WAIT_BUSY;
//Select the controller
writeCMD(0x13);
//Jump over BMP header
bmp_file.seek(54);
//grab one row of pixels from the SD card at a time
static uint8_t one_line[HRES / 2 * 3];
for (int line = 0; line < VRES * 2; line++)
{
//Set the LCD to the left of this line. BMPs store data
//to have the image drawn from the other end, uncomment the line below
//read a line from the SD card
bmp_file.read(one_line, HRES / 2 * 3);
//send the line to the display
send_pixels_BW(HRES / 2 * 3, one_line);
}
Serial.println("refreshing......");
//Write the command: Display Refresh (DRF)
fullUpdate();
//Make sure the display is not busy before starting a new command.
WAIT_BUSY;
Serial.print(" complete");
//Give a bit to let them see it
delay(3000);
}
}
}
//Release the BMP file handle
bmp_file.close();
}
//Release the root directory file handle
root_dir.close();
}
//================================================================================
void Load_Flash_Image_To_Display_RAM_RLE(uint16_t width_pixels,
uint16_t height_pixels,
const uint8_t *BW_image)
{
//Index into *image, that works with pgm_read_byte()
uint8_t count = 0;
//Get width_bytes from width_pixel, rounding up
uint8_t
width_bytes;
width_bytes = (width_pixels + 7) >> 3;
//Make sure the display is not busy before starting a new command.
WAIT_BUSY;
//Select the controller
ePaper_CS_0;
//Aim at the command register
ePaper_DC_0;
// Write RAM (Black White) / RAM 0x24
// After this command, data entries will be
// written into the BW RAM until another
// command is written. Address pointers will
// advance accordingly
SPI.transfer(0x24);
//Pump out the data.
ePaper_DC_1;
count = 0;
for (int i = 0; i < MONO_ARRAY_SIZE; i = i + 2)
{
count = pgm_read_byte(&BW_image[i]);
for (uint8_t j = 0; j < count; j++)
SPI.transfer(pgm_read_byte(&BW_image[i + 1]));
}
fullUpdate();
//Deslect the controller
ePaper_CS_1;
}
//================================================================================
void Load_Flash_Image_To_Display_RAM(uint16_t width_pixels,
uint16_t height_pixels,
const uint8_t *BW_image)
{
//Index into *image, that works with pgm_read_byte()
uint8_t count = 0;
//Get width_bytes from width_pixel, rounding up
uint8_t
width_bytes;
width_bytes = (width_pixels + 7) >> 3;
//Make sure the display is not busy before starting a new command.
WAIT_BUSY;
//Select the controller
ePaper_CS_0;
//Aim at the command register
ePaper_DC_0;
// Write RAM (Black White) / RAM 0x24
// After this command, data entries will be
// written into the BW RAM until another
// command is written. Address pointers will
// advance accordingly
SPI.transfer(0x24);
//Pump out the data.
ePaper_DC_1;
count = 0;
for (int i = 0; i < MONO_ARRAY_SIZE; i++)
{
SPI.transfer(pgm_read_byte(&BW_image[i]));
}
fullUpdate();
//Deslect the controller
ePaper_CS_1;
}
//================================================================================
void send_pixels_BW(uint16_t byteCount, uint8_t *dataPtr)
{
uint8_t data;
uint8_t red;
uint8_t green;
uint8_t blue;
while (byteCount != 0)
{
uint8_t data = 0;
red = *dataPtr;
dataPtr++;
byteCount--;
green = *dataPtr;
dataPtr++;
byteCount--;
blue = *dataPtr;
dataPtr++;
byteCount--;
if (150 > ((red * .21) + (green * .72) + (blue * .07)))
{
data = data | 0x01;
}
for (uint8_t i = 0; i < 7; i++)
{
red = *dataPtr;
dataPtr++;
byteCount--;
green = *dataPtr;
dataPtr++;
byteCount--;
blue = *dataPtr;
dataPtr++;
byteCount--;
data = data << 1;
if (127 > ((red * .21) + (green * .72) + (blue * .07)))
{
data = data | 0x01;
}
else
{
data = data & 0xFE;
}
}
writeData(data);
}
}
void outDeepSleep()
{
//Software Reset
WAIT_BUSY;
writeCMD(0x12);
WAIT_BUSY;
writeCMD(0x10);
writeData(0x00);
}
void deepSleep()
{
writeCMD(0x10);
writeData(0x01);
}
//=============================================================================
#define SHUTDOWN_BETWEEN_UPDATES (0)
#define waittime 5000
#define splashscreen 1
#define partialUpdate 1
#define showBMPs 0
#define black 1
#define white 1
void loop()
{
Serial.println("top of loop");
#if splashscreen
initEPD();
//load an image to the display
Load_Flash_Image_To_Display_RAM(HRES, VRES, Mono_1BPP);
Serial.print("refreshing . . . ");
WAIT_BUSY;
Serial.println("refresh complete");
//for maximum power conservation, power off the EPD
delay(waittime);
#endif
#if partialUpdate
initEPD();
setBaseMap(Mono_1BPP);
WAIT_BUSY;
delay(100);
partialUpdateCharacters(Mono_Letter_C);
partialUpdateCharacters(Mono_Letter_F);
partialUpdateCharacters(Mono_Letter_A);
partialUpdateCharacters(Mono_Letter_P);
delay(waittime);
#endif
#if showBMPs
//BMPs are inverted
initEPD();
Epaper_Write_Command(0x01); //Driver output control
Epaper_Write_Data(0xF9);
Epaper_Write_Data(0x00);
Epaper_Write_Data(0x01);
show_BMPs_in_root();
delay(waittime);
//flip the display back to normal
Epaper_Write_Command(0x01); //Driver output control
Epaper_Write_Data(0xF9);
Epaper_Write_Data(0x00);
Epaper_Write_Data(0x00);
#endif
#if black
initEPD();
//Make sure the display is not busy before starting a new command.
WAIT_BUSY;
//Select the controller
ePaper_CS_0;
//Aim at the command register
ePaper_DC_0;
// Write RAM (Black White) / RAM 0x24
// After this command, data entries will be
// written into the BW RAM until another
// command is written. Address pointers will
// advance accordingly
SPI.transfer(0x24);
//Pump out the data.
ePaper_DC_1;
for (int i = 0; i < MONO_ARRAY_SIZE; i++)
{
SPI.transfer(0xff);
}
fullUpdate();
//Deslect the controller
ePaper_CS_1;
delay(waittime);
#endif
#if white
initEPD();
//Make sure the display is not busy before starting a new command.
WAIT_BUSY;
//Select the controller
ePaper_CS_0;
//Aim at the command register
ePaper_DC_0;
// Write RAM (Black White) / RAM 0x24
// After this command, data entries will be
// written into the BW RAM until another
// command is written. Address pointers will
// advance accordingly
SPI.transfer(0x24);
//Pump out the data.
ePaper_DC_1;
for (int i = 0; i < MONO_ARRAY_SIZE; i++)
{
SPI.transfer(0x00);
}
fullUpdate();
//Deslect the controller
ePaper_CS_1;
delay(waittime);
#endif
}
//=============================================================================
here is the compiler output
FQBN: Seeeduino:nrf52:xiaonRF52840Sense
Using board 'xiaonRF52840Sense' from platform in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\Seeeduino\hardware\nrf52\1.1.1
Using core 'nRF5' from platform in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\Seeeduino\hardware\nrf52\1.1.1
Linking everything together...
"C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\Seeeduino\\tools\\arm-none-eabi-gcc\\9-2019q4/bin/arm-none-eabi-gcc" "-LC:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\5F57683B010A56727E94AB4AF4618B60
"C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\Seeeduino\\hardware\\nrf52\\1.1.1/tools/adafruit-nrfutil/win32/adafruit-nrfutil.exe" dfu genpkg --dev-type 0x0052 --sd-req 0x0123 --application "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\5F57683B010A56727E94AB4AF4618B60/CFAP122250A20213.ino.hex" "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\5F57683B010A56727E94AB4AF4618B60/CFAP122250A20213.ino.zip"
Zip created at C:\Users\Dude\AppData\Local\Temp\arduino\sketches\5F57683B010A56727E94AB4AF4618B60/CFAP122250A20213.ino.zip
Using library epd4in2 at version 1.0 in folder: D:\Arduino_projects\libraries\epd4in2-demo
Using library SPI at version 1.0 in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\Seeeduino\hardware\nrf52\1.1.1\libraries\SPI
Using library SD at version 1.2.4 in folder: C:\Users\Dude\AppData\Local\Arduino15\libraries\SD
Using library Adafruit TinyUSB Library at version 1.7.0 in folder: C:\Users\Dude\AppData\Local\Arduino15\packages\Seeeduino\hardware\nrf52\1.1.1\libraries\Adafruit_TinyUSB_Arduino
"C:\\Users\\Dude\\AppData\\Local\\Arduino15\\packages\\Seeeduino\\tools\\arm-none-eabi-gcc\\9-2019q4/bin/arm-none-eabi-size" -A "C:\\Users\\Dude\\AppData\\Local\\Temp\\arduino\\sketches\\5F57683B010A56727E94AB4AF4618B60/CFAP122250A20213.ino.elf"
Sketch uses 58220 bytes (7%) of program storage space. Maximum is 811008 bytes.
Global variables use 7912 bytes (3%) of dynamic memory, leaving 229656 bytes for local variables. Maximum is 237568 bytes.
Serial output looks like this.
SD could not initialize
setup complete
top of loop
refreshing . . . refresh complete
top of loop
refreshing . . . refresh complete
top of loop
refreshing . . . refresh complete
top of loop
refreshing . . . refresh complete
HTH
GL
PJ
Nice Display for sure.!
![]()