I’m looking for a simple example of using the onboard grove connectors, or even the grove shield if necessary.  The lorawan part works great, but I can’t get any readings from external sensors.   Looking for a simple soil moisture sensor example.
thanks.
Hi, 
here is the code for reading the Soil Moisture.
[code]int sensorPin = A0;
int sensorValue = 0;
void setup() {
Serial.begin(9600);
}
void loop() {
// read the value from the sensor:
sensorValue = analogRead(sensorPin);
Serial.print("Moisture = " );
Serial.println(sensorValue);
delay(1000);
}[/code]
Here we are connected Soil Moisture sensor on the  A0  Pin, and you can change that if you want. more resource: http://wiki.seeedstudio.com/Grove-Moisture_Sensor/
OK. Thank you.  I thought it was a problem with the board, but it was just my mistake on the output.  I had serial.print rather then serialUSB.print and it was stopping at that line.
thanks.
It is a common and valuble mistake. Thanks for pointing it out!