Hi All,
I installed a GPS Bee onto my Stalker 3.1 and I struggle to make it work.
The GPS Bee works perfectly with the UartSBee v5 and the u-center. I do get a signal. All fine here.
My troubles begin when I fix the GPS Bee onto the Stalker. I use the pins 0/1 , pin 9 for electricity and TinyGPS as library. - and i am getting no info from the GPS module in the serial display. How can that be? i really have no idea, and i would be very happy if somebody could give me an idea of what to do or where to look at.
Thanks a lot!
and the code is here:
#include <SoftwareSerial.h>
#include <TinyGPS++.h>
/*
This sample sketch demonstrates the normal use of a TinyGPS++ (TinyGPSPlus) object.
It requires the use of SoftwareSerial, and assumes that you have a
4800-baud serial GPS device hooked up on pins 4(rx) and 3(tx).
*/
int RXPin = 0;
int TXPin = 1;
static const uint32_t GPSBaud = 9600;
// The TinyGPS++ object
TinyGPSPlus gps;
// The serial connection to the GPS device
SoftwareSerial ss(RXPin, TXPin);
void setup()
{
pinMode(9, OUTPUT);
Serial.begin(9600);
ss.begin(GPSBaud);
Serial.println(F(“DeviceExample.ino”));
Serial.println(F(“A simple demonstration of TinyGPS++ with an attached GPS module”));
Serial.print(F(“Testing TinyGPS++ library v. “)); Serial.println(TinyGPSPlus::libraryVersion());
Serial.println(F(“by Mikal Hart”));
Serial.println();
}
void loop()
{ digitalWrite(9, HIGH);
// This sketch displays information every time a new sentence is correctly encoded.
while (ss.available() > 0)
if (gps.encode(ss.read()))
displayInfo();
if (millis() > 5000 && gps.charsProcessed() < 10)
{
Serial.println(F(“No GPS detected: check wiring.”));
while(true);
}
}
void displayInfo()
{
Serial.print(F(“Location: “));
if (gps.location.isValid())
{
Serial.print(gps.location.lat(), 6);
Serial.print(F(”,”));
Serial.print(gps.location.lng(), 6);
}
else
{
Serial.print(F(“INVALID”));
}
Serial.print(F(” Date/Time: “));
if (gps.date.isValid())
{
Serial.print(gps.date.month());
Serial.print(F(”/”));
Serial.print(gps.date.day());
Serial.print(F("/"));
Serial.print(gps.date.year());
}
else
{
Serial.print(F(“INVALID”));
}
Serial.print(F(" “));
if (gps.time.isValid())
{
if (gps.time.hour() < 10) Serial.print(F(“0”));
Serial.print(gps.time.hour());
Serial.print(F(”:"));
if (gps.time.minute() < 10) Serial.print(F(“0”));
Serial.print(gps.time.minute());
Serial.print(F(":"));
if (gps.time.second() < 10) Serial.print(F(“0”));
Serial.print(gps.time.second());
Serial.print(F("."));
if (gps.time.centisecond() < 10) Serial.print(F(“0”));
Serial.print(gps.time.centisecond());
}
else
{
Serial.print(F(“INVALID”));
}
Serial.println();
}