I have just installed arduino-0022 for the Mac to use with the Seeeduino ADK main board. The software came with an FTDI USB serial driver package 10_4_10_5_10_6 which I installed. The Arduino software assembles the demokit example OK, but crashes when uploading to the board with the following error report showing a java exception. There seem to have been previous reports on the internet of FTDI Mac problems (Snow Leopard). Does anyone have a fix for the problem?
Tony
Process: JavaApplicationStub [80131]
Path: /Volumes/Arduino/Arduino.app/Contents/MacOS/JavaApplicationStub
Identifier: cc.arduino.Arduino
Version: 0022 (0022)
Code Type: X86 (Native)
Parent Process: launchd [219]
Date/Time: 2011-07-23 22:36:46.538 +0100
OS Version: Mac OS X 10.6.7 (10J869)
Report Version: 6
Interval Since Last Report: 599573 sec
Crashes Since Last Report: 10
Per-App Interval Since Last Report: 3599 sec
Per-App Crashes Since Last Report: 10
Anonymous UUID: 6E6D059F-D183-4E0C-A566-1804491FCA7C
Exception Type: EXC_BAD_ACCESS (SIGSEGV)
Exception Codes: KERN_INVALID_ADDRESS at 0x00000000b1d35be0
Crashed Thread: 22 Java: Thread-86