Seeed Studio XIAO nRF52840 Sense X axis and Y axis orientation

Seeed Studio XIAO nRF52840 Sense with built in IMU; what is the X axis and Y axis orientation of the board?

Thanks,
Gentry

just fire up the demo and you should be able to figure it out

cgwaltney,
Will do. Thanks!

Hi there,
So take a look at this IMU parked demo, Keep in mind the z is from the floor.
HTH
GL :slight_smile: PJ :v:

Thanks again from our resident Nordic Cheerleader!

Remember the Right hand rule…

1-Right hand fingers point to positive X
2-Curl fingers toward positive y
3-Thumb will naturally point in positive Z

PJ_Glasso,

Thank you, very informative!

cgwaltney,

Thanks, that helps!