Seeed Studio XIAO ESP32-S3 Camera Module Reboot loop with CameraWebServer example

Hello,

I am trying to figure out why i cannot get the built in example sketch for the CameraWebServer to run of the Seeed Studio XIAO ESP32-S3 Camera Module. I am using arduino IDE, i installed and updated the esp32 board manager stuff

I get a reboot loop with the following error info.

entry 0x403c88b8

Guru Meditation Error: Core  1 panic'ed (LoadProhibited). Exception was unhandled.

Core  1 register dump:
PC      : 0x420502b5  PS      : 0x00060730  A0      : 0x82047d8a  A1      : 0x3fcebf30  
A2      : 0x3fcec480  A3      : 0x3fcec018  A4      : 0xffff8fff  A5      : 0x3fc96e98  
A6      : 0x3c0ca834  A7      : 0x00000001  A8      : 0x3c0ca898  A9      : 0x00000000  
A10     : 0x00000019  A11     : 0x00000060  A12     : 0x00000060  A13     : 0x00060323  
A14     : 0x00000004  A15     : 0x0000abab  SAR     : 0x0000001c  EXCCAUSE: 0x0000001c  
EXCVADDR: 0x00000000  LBEG    : 0x400570e8  LEND    : 0x400570f3  LCOUNT  : 0x00000000  


Backtrace: 0x420502b2:0x3fcebf30 0x42047d87:0x3fcebf80 0x420477a9:0x3fcebfb0 0x42002e99:0x3fcec010 0x420093aa:0x3fcec0c0 0x4037dffd:0x3fcec0e0




ELF file SHA256: 1c71aa485

Rebooting...

Here are the parameters i am using for the board settings

I’ve seen other posts about boot loop issues but none that seem to match this error.

Anything anyone could help point me in the right direction to get that working?

Thanks!

Ok I got to a new error which is good, I had to go to the board_config.h whihc is part of the CameraWebServer example. I changed what originally was set as CAMERA_MODEL_ESP_EYE and switched to CAMERA_MODEL_ESP32S3_EYE and now I get a “Camera init failed with error 0x106” not sure the config switch was right but the seeed one I have is the s3 and I got a new error so I’m going to assume that is progress unless someone tells me otherwise.

Ok i saw there is one in the board_config.h that is for XIAO_ESP32S3 and that got the default program working

Check the camera model and PSRAM.

#define CAMERA_MODEL_XIAO_ESP32S3 // Uncomment this line in board_config.h

Board: XIAO_ESP32S3
Flash Size: 8MB
PSRAM: OPI PSRAM

Hi there,

Worth Noting the “BSP” matters with this Demo :v:
Be sure it’s the correct one.
Roll it back to the older one listed in the Demo I posted.

HTH
GL :slight_smile: PJ :v: