SEEED Solar Node and MQTT issues

Attempting to setup MQTT, FAILS! In the LoRa setting; Advanced, the ignore MQTT is Disabled. Ok to MQTT is Enabled and Transmit Enabled is Enabled.

Then went to the MQTT module and ENABLED the MQTT enable. Then a message pops up saying 0% or Quit. After 5 minutes it still says 0%. Quit, as I found out has no effect. Then I noticed that my Node is no longer ONLINE.
This is a new area and I could not find any links that would help. I hope the Community can help me understand what I am doing wrong.

Using Bluetooth, on my Android phone It seems that when you change almost any setting the Solar Node reboots, and the 0% shows up but does nothing, and I close it. It takes between 20 and 90 seconds before you can reconnect. I can see in the lower right-hand corner of that box when it starts do stuff with modules, and then it counts nodes before it shows that it’s connected.

Or, is says the setting has taken and doesn’t reboot.

Perhaps someone with more knowledge about the MQTT problem will comment.

Allow MQTT is under Advanced, and this lets you turn it on in Settings.