I have 3 Seeed AWS IoT buttons that were properly configured and working (would transmit to the AWS cloud and flash green). I had a power outage that rebooted the router. After power came back and was stable that, Internet is working but the buttons no longer transmit; when pressed, they flash orange.
- Do need to re-setup all the buttons to get them to reconnect?
- What exactly goes wrong when power is lost? Obviously the buttons are battery powered and the router comes back up successfully. Are the buttons reserving DHCP addressed that they lose, or losing a STUN configuration?
Thanks!