Hi, can someone help how to have the code in lambda to get the click type? Right now each time i click i get undefined. What shall i pass to be able to get the click type and than act depending on it?
Thank you in advance
Hi, can someone help how to have the code in lambda to get the click type? Right now each time i click i get undefined. What shall i pass to be able to get the click type and than act depending on it?
Thank you in advance
Hi! I also have a question surrounding click payloads. When i use the seeed button to trigger a lambda, i don’t see an option to use double click or long click to trigger the lambda. Can i use each type of click to trigger a different lambda? Or do i need to get the button click payload and take action in my code based on it being a single, double, or long click?
Hi, I also have similar situation, do you know what is it the default topic for the Seeed Button AWS, I had try with iotbutton similar to aws iot button for using with the mqtt protocol, but when I clicked it i could not get the payload also can’t trigger any lamba function and off course can not get the click type and its serial number
Hi guys. It doesn’t seem like this forum is really moderated by anyone from SEEED. Which is a little depressing. Post here if you make any progress on figuring out the different payload types. If you know the default topic for the button - that would be great too so I can see the payloads.
Not sure if you’ve solved this but the examples in the IOT mailer lambda etc. show undefined as the click type is nested in the JSON not at the top level. I solved this by just parsing the JSON
See below for an example which will let you see what’s happening in cloudwatch:
exports.handler = function(event, context) {
var msg = JSON.stringify(event);
console.log(msg);
var jsonmsg = JSON.parse(msg);
if (jsonmsg.deviceEvent.buttonClicked.clickType == ‘SINGLE’){
console.log(‘Single Click’);
}
};
The Seeed IoT Button for AWS supports three types of clicks: single, double, and long press , and 3 LEDs for different indications. These buttons support replaceable and rechargeable batteries. spacebar counter The Seeed IoT Button For AWS is a Wi-Fi-based, programmable button* that deploys the AWS IoT 1-Click service. The simple Wi-Fi device is easy … The *Seeed IoT Button for AWS supports three types of clicks : single, double, and long press, and 3 LEDs for different indications. AWS Service. AWS IoT Core.