I have seeduino film with
UARTSB FRAME
OLED FRAME
BLUETOOTH
I connected the units as instructed in wiki pages
I load the Bluetooth sketch file example to arduino 1.01 compiler
I selected the board as “Arduino mini 3V3 atmega168 8mhz”
I checked the UARTSB board by bridging Tx & Ty it works fine.
I received the following messages during uploading, which means a lack of communication between the PC and the Seeeduino film.
Binary sketch size: 2.352 bytes (of a 14.336 byte maximum)
avrdude: stk500_getsync(): not in sync: resp=0x00
Where did I go wrong ?
regards Serdar