This website https://www.seeedstudio.com/XIAO-ESP32S3-p-5627.html hints that the Seed XIAO ESP32-S3 can be used with MicroPython but gives zero guide how to.
Does anyone know how to achive this? Which MicroPython build (bin or u2f) should be used and how to put the device into bootloader mode?
Or is MicroPython a planned support and it will come in the future? Is there a plan for a CircuitPython port as well? (I would prefer CircuitPython over MicroPython.)
MicroPython v1.20.0 on 2023-04-26; ESP32S3 module (spiram octal) with ESP32S3
Type "help()" for more information.
Havenât made any tests yet.
Serial port baud rate seems to be 9600.
To enter the bootloader mode press and hold down the teen- tiny boot button that is further from the red led. Then press the button close to the red led then release the first button.
How is that an answer to the question: âHow to install MicroPython on Seed XIAO ESP32-S3?â
That is an answer to the question: âHow to use Seed XIAO ESP32-S3 with Arduino IDE?â
Arduino is C/C++, MicroPython (and CircuitPython) is close to python. Different programming languagesâŚ
Hi Olibali,
From what I have seen here there isnât any support for Circuit Python or even the Micro Python. They seem to be fast and loose with the specs and compatibility stuff here. YMMV. The answers are some time so basic they donât address the issues. Other Users However may know more, also Adfruit may provide some info if you post over there what issues your having or info you need to know. Lots of smart folks here and there.
HTH
GL
PJ
its a good fast and loose with the specs and compatibility stuff here. YMMV. The answers are some time so basic they donât address the issues. Other Users However may know more, also Adfruit may provide some info if you post over there what issues your having or info you need to know. Lots of smart folks here and there.