Dear Support Team,
I hope this message finds you well. I am writing to seek assistance with a recurring issue I’ve been experiencing with the Seed Studio Nano host hotspot. The hotspot connection frequently disconnects without any apparent reason, and I’m seeking guidance on how to resolve this problem.
To provide you with more information,
Hardware Configuration:
SKU : 110061362
Module: Jetson Nano 4GB Carrier Board Operating System:J1010 Carrier Board Power Interface: Type-C connector
wi-fi module configuration:
WIFI-module name : Intel Dual Band Wireless2.4/5GHz Bluetooth 4.2 WiFi Card 867 Mbps for 8265 AC AC8265
TX/RX Streams 2x2
Bands 2.4, 5 GHz
Max Speed 867 Mbps
Description of the Issue:
When I enable the host hotspot on the Seed Studio Nano, it establishes a connection successfully.
However, after a variable period of time the hotspot connection disconnects.
This issue occurs consistently, and I have experienced it on multiple occasions. I have verified that the hotspot settings on the Seed Studio Nano are configured correctly.
Thank you for your attention to this matter. I look forward to your prompt response.
regards,
Hari Prasath