🄽 See the Future, Building AI reGoggles - First to Open Source

Building AI Goggles — What its ā€œBrainā€ Should Look Like

:goggles: :backhand_index_pointing_left: :grin:

This thing is WOW, Nutz…
Check out the Vlog and I hope they come in priced right…

reGoggles VLOG!!

2.4 HD streaming, 4K still capture

The V881M3-WB2 encodes H.265 at 4K@30 and H.264 at 4K@25, but reGoggles doesn’t stream 4K continuously: 1T1R single-stream Wi-Fi can’t sustain the bitrate, and the sealed temple’s short thermal path would force throttling under sustained high-bitrate encoding. Testing shows long-running streams hold 1080p, where latency and stability for on-device inference and remote views are more predictable. 4K is reserved for still captures — key-moment records and high-resolution vision-model input.

Spec’s are pretty sweet for entry level device. Life/Safety, Search and rescue, How to Coach mode in the goggles… Get ready for the middle Tech , before the robots take over , Augmented reality with ā€œvirtual projectionā€ :trade_mark: is coming :crossed_fingers:

the all-in one device is pretty serious miniaturization, two pieces make the complete system.

It’s a reWorld…:slight_smile:
" So I was ā€œreThinkingā€ about that chaotic morning when my rePhone locked up right as I tried to sync my reComputer logs. I figured I’d grab my recamera to snap some macro shots of the fried board and slip on my reGoggles to check the schematic overlay.

Just as I tied everything into the reServer to pull a clean recovery image, my reRouter dropped its connection entirely—sending my whole desk into total re-volt right before my morning coffee !

HTH
GL :slight_smile: PJ :v: