Hi brilliant members here.
I feel give up with 2.8 TFT SDCARD to list all file in micro card. I just using standard sd card code and just include tftv2.h and spi.h. But still didnot have any file to appear at serial monitor. What is the problem with this standard code? Need help please.
[code]/*
SD card basic file example
This example shows how to create and destroy an SD card file
The circuit:
- SD card attached to SPI bus as follows:
** MOSI - pin 11
** MISO - pin 12
** CLK - pin 13
** CS - pin 4
created Nov 2010
by David A. Mellis
modified 9 Apr 2012
by Tom Igoe
This example code is in the public domain.
*/
#include <SD.h>
#include <SPI.h>
#include <TFTv2.h>
Sd2Card card;
File root;
void setup()
{
// Open serial communications and wait for port to open:
Serial.begin(9600);
while (!Serial) {
; // wait for serial port to connect. Needed for Leonardo only
}
Serial.print(“Initializing SD card…”);
// On the Ethernet Shield, CS is pin 4. It’s set as an output by default.
// Note that even if it’s not used as the CS pin, the hardware SS pin
// (10 on most Arduino boards, 53 on the Mega) must be left as an output
// or the SD library functions will not work.
pinMode(10, OUTPUT);
card.init(SPI_FULL_SPEED,4);
if (!SD.begin(10)) {
Serial.println(“initialization failed!”);
return;
}
Serial.println(“initialization done.”);
root = SD.open("/");
printDirectory(root, 0);
Serial.println(“done!”);
}
void loop()
{
// nothing happens after setup finishes.
}
void printDirectory(File dir, int numTabs) {
while(true) {
File entry = dir.openNextFile();
if (! entry) {
// no more files
//Serial.println("**nomorefiles**");
break;
}
for (uint8_t i=0; i<numTabs; i++) {
Serial.print('\t');
}
Serial.print(entry.name());
if (entry.isDirectory()) {
Serial.println("/");
printDirectory(entry, numTabs+1);
} else {
// files have sizes, directories do not
Serial.print("\t\t");
Serial.println(entry.size(), DEC);
}
entry.close();
}
}
[/code]