S2120 new software version V2.1

Had some problems with bluetooth connection, tried all kind of things, then I saw in the app that there was a new SW-version 2.1 for the S2120. Downloaded it, and problems are gone.

I dont know what else it does. Have not found out.

Worked for a day or three. Now I cannot connect the bluetooth from Android phone to s2120. Tried all known psw’s, 0000, 000000, 1234, 123456. Any other ideas? Tried with two different phones.
I dont want to put back the unit on top of the roof before this is solved.:slight_smile:

Again I answer myself, in case somebody runs into the same problem regardig bluetooth connection.

  1. Remove batteries in S2120.
  2. Cover the solar panel w/ something like a towel or dark paper.
  3. Wait a day or three so the S2120 totally don’t have any power left.
  4. This seems to clear internal memories.
  5. Keep solar panel covered, install new batteries.Now you can remove the solar panel cover.
  6. Connect to S2120 w/ bluetooth, configure it as normal.
  7. You might do some testing before climbing up the ladder!

This worked for me. Did not have to put it in the garbage bin!