S2120 data error

I am sending the data from an S2120 in the other server option, we are sending it to a private server, it has been working well for 10 days, since yesterday it started showing an error in the second part of data which includes rain rate and atmospheric pressure, The other data is normal, this is the error code, can anyone help me? I do not have physical access to it as it is more than 300km away

“root”:[

1 item

0:{

4 items

“measurementId”:

string"4101"

“type”:

string"sensor_error_event"

“errCode”:

string"0E"

“descZh”:

string"CCL_SENSOR_DATA_VALUE_MISSED"

}

]