S2100 failed to join lora network

I think the lorawan gateway is the main problem. None of my sensors are connected to the network. All of them went offline

did you http into the gateway and check the setup… the LoRa Frequency region?

My lorawan is not an M2 gateway.

I use lorawan gateway with model -
LoRa-G-868-E/4G

This is what I get when i try to login via IP address of the gateway.


i am gonna try to get someone from seeed to reach out to you

Thanks. Also can I factory reset the gateway?

Or even just the lora module to be factory reset

i have heard factory reset makes it worse so dont try that yet

What to do then? Please i need help on this. My project won’t work unless this problem is solve.

all i can do is try to help you troubleshoot… please post a
list of what you have done

Can you check if you’re using Seeed’s Sever? please enable this button

Yeah I’m using seeed’s server

Still waiting for reply. Please anyone from seeed studio? I’m struggling to finished my research project because of this issue.
I bought sensecap product because of its accuracy and its user friendly features so please help me with this issue. Thank you

Hi there,
I think they are on holiday until the 17th SO hang in there, someone will respond.
GL :slight_smile: PJ :v:

Still waiting for support

Where’s the support from seeed here? How to can i get support from them?

to get support you have to email them… this is more or less peer to peer help…