Rtsp for xiaoesp32s3?

Helloo,

May I ask how to find the rtsp for the xiaoesp32 camera? I want to set it up on obs like this https://www.youtube.com/watch?v=PNAOFDjE_cY

Hi there,
Well the camera isn’t a packaged ,IP camera , The camera server software makes it stream, you would need to add the port in the code or See if OBS will take the stream directly from it. Have a look at the Web Camera demo and perhaps there is a hint in there.
HTH
GL :slight_smile: PJ

okayy

i was trying to set up rtsp using this tutorial https://www.youtube.com/watch?v=Krx_z3TuW0w&t=27s
but i get this error
SPIRam Total heap 0, SPIRam Free Heap 0

ChipRevision 0, Cpu Freq 240, SDK Version v4.4.6-dirty

Flash Size 8388608, Flash Speed 80000000

##################################

Guru Meditation Error: Core 1 panic’ed (LoadProhibited). Exception was unhandled.

do you know how to fix this?

Hi there,
Turn on the PSram in the tools section. Check all the options are correct.
HTH
GL :slight_smile: PJ