Round Display with Xiao Nrf52840 Sense ,TFT_eSPI , LVL Example

I managed to get something out of this, it will detect screen touches–but when I load the next demo I see this.

Build:Feb  7 2021
rst:0x8 (TG1WDT_SYS_RST),boot:0x8 (SPI_FAST_FLASH_BOOT)
Saved PC:0x40380082
SPIWP:0xee
mode:DIO, clock div:1
load:0x3fcd5820,len:0x1058
load:0x403cc710,len:0x8a8
load:0x403ce710,len:0x2fac
entry 0x403cc710
ESP-ROM:esp32c3-api1-20210207

So now its continuously crashing the ESP32C3 I got plugged in? This is code it is running…

#include <TFT_eSPI.h>
#include <SPI.h>
#define USE_TFT_ESPI_LIBRARY
#include "lv_xiao_round_screen.h"

lv_coord_t touchX, touchY;

void setup() {
  // put your setup code here, to run once:
  Serial.begin(115200);

  pinMode(TOUCH_INT, INPUT_PULLUP);
  Wire.begin();
  
  // Initialise the screen
  tft.init();

  tft.setRotation(0);
  tft.fillScreen(TFT_BLACK);
}

void loop() {
  // put your main code here, to run repeatedly:
  if(chsc6x_is_pressed())
  {
    Serial.println("The display is touched.");
    chsc6x_get_xy(&touchX, &touchY);
    tft.drawCircle(touchX, touchY, 15, TFT_WHITE);
  }
  
  delay(50);
}