Round Display with Xiao Nrf52840 Sense ,TFT_eSPI , LVL Example

Hi there,
Something I notice that appears to be a common OVERSITE when using or testing with the
TFT_eSPI lib. The examples include a Diagnostic from the Author that is meant to be run after the edits are made to verify what the LIB recognises as setup.

“READ_USER_SETUP.ino”
Do not proceed further if it doesn’t look like it should or if it does NOT run at all , it means you knurled it Up.
You should receive a serial output like this:

[code]
TFT_eSPI ver = 2.5.23
Processor    = ESP32
Frequency    = 160MHz
Transactions = Yes
Interface    = SPI
Display driver = 9A01
Display width  = 240
Display height = 240

MOSI    = GPIO 10
MISO    = GPIO 9
SCK     = GPIO 8
TFT_CS   = GPIO 3
TFT_DC   = GPIO 5

TFT_BL           = GPIO 21

Font GLCD   loaded
Font 2      loaded
Font 4      loaded
Font 6      loaded
Font 7      loaded
Font 8      loaded
Smooth font enabled

Display SPI frequency = 40.00
[/code]

This is the process I use and it get’s me there EVERY Time!
HTH
GL :slight_smile: PJ
:v: