Is there anywhere I can download the original firmware/programming for the LED cube? After uploading the updated Rainbowduino v3h firmware and one of the test sketches using the new Arduino v1.0 environment, I can’t get many of the PDE sketches to work and I want to return it to the original configuration. And are there any updates that are compatible to work with the Arduino 1.0 software?
Dear customer,
There is Arduino 1.0 libraries on our WIKI.
seeedstudio.com/wiki/Rainbowduino_v3.0
But do you use Rainbowduino 2.0?
And what version about your board?
Here is the WIKI for Rainbowduino 2.0 seeedstudio.com/wiki/Rainbowduin … Atmega_328.
But sorre there is no 1.0 code yet, and better you can refer to Arduino to know what change with 0023 to 1.0.
Best regars,
Yuri
I have the newest boxed retail version (assembled) of the Cube with Rainbowduino board v3. Do you have the original software (i.e. light up patterns) that was preloaded available to redownload?
Dear customer,
I not sure what codes you want. But actually there is all code in the libraries which on WIKI.
Best regards,
Yuri
So do you know which PDE sketch (i.e. cube1, moodcube, etc.) was the default one that played when you plugged it in the first time?
Hi there,
seeedstudio.com/wiki/Rainbow … e%29#Demos
On the WIKI there are some demo code, we also use them to test it.
So hope you can find what you want.