RFBee and transmission distance

Hi friends,

The max transmit range of the RFBee is listed below:
Indoor/Urban: up to 50m
Outdoor line-of-sight: up to 120m

Maybe you can try using the AT command “PA” to increase the transmitting power, thus expanding the transmit range.
For the use of AT command,refer to the file “RFBee User Manual” listed at the bottom of the wiki page:http://www.seeedstudio.com/wiki/index.php?title=RFbee_V1.1_-_Wireless_Arduino_compatible_node

Thanks!