I want to edit and add some tabs on the main reTerminal DM dashboard (the one that appears right after startup see picture below).
Right now, there are 3 tabs:
- Node-RED dashboard
- Node-RED environment
- Settings
I want to customize this dashboard like this:
- Add more dashboards for Node-RED.
- Add Grafana button so that it will show Grafana.
- Password protection of the settings.
Is there any way I can do that? Adding more dashboards and Grafana could be something like a simple iFrame.
My main question is how and where I can change the code / appearance of the main dashboard of the reTerminal DM?
Thank you in advance!