Hi all, my boot/config.txt has 2 lines added to the end of the file, each per reTerminal documentation.
One is to make the touchscreen rotation correct (dtoverlay=reTerminal,tp_rotate=1) and the other is for activation of the buttons and other onboard components on the older MCP23008 chip (dtoverlay=reTerminal,addr=0x20,mcp23008).
Each line works great… but only if I put it LAST in the config.txt. Whichever line is printed LAST in the file gets applied and the other does not.
(In other words, if the buttons line is placed last in the file, the front buttons work but the touchpad rotation is wrong. And if I place the touchpad rotation line last in the file, the front buttons stop working but the touchpad rotation is correct.)
Any ideas why or how can I make both of these apply? I need the buttons and I need the touchscreen.
Thanks! Full file below.
# For more options and information see
# http://rpf.io/configtxt
# Some settings may impact device functionality. See link above for details
# uncomment if you get no picture on HDMI for a default "safe" mode
#hdmi_safe=1
# uncomment the following to adjust overscan. Use positive numbers if console
# goes off screen, and negative if there is too much border
#overscan_left=16
#overscan_right=16
#overscan_top=16
#overscan_bottom=16
# uncomment to force a console size. By default it will be display's size minus
# overscan.
#framebuffer_width=1280
#framebuffer_height=720
# uncomment if hdmi display is not detected and composite is being output
#hdmi_force_hotplug=1
# uncomment to force a specific HDMI mode (this will force VGA)
#hdmi_group=1
#hdmi_mode=1
# uncomment to force a HDMI mode rather than DVI. This can make audio work in
# DMT (computer monitor) modes
#hdmi_drive=2
# uncomment to increase signal to HDMI, if you have interference, blanking, or
# no display
#config_hdmi_boost=4
# uncomment for composite PAL
#sdtv_mode=2
#uncomment to overclock the arm. 700 MHz is the default.
#arm_freq=800
# Uncomment some or all of these to enable the optional hardware interfaces
dtparam=i2c_arm=on
#dtparam=i2s=on
dtparam=spi=on
# Uncomment this to enable infrared communication.
#dtoverlay=gpio-ir,gpio_pin=17
#dtoverlay=gpio-ir-tx,gpio_pin=18
# Additional overlays and parameters are documented /boot/overlays/README
# Enable audio (loads snd_bcm2835)
dtparam=audio=on
# Automatically load overlays for detected cameras
camera_auto_detect=1
# Automatically load overlays for detected DSI displays
display_auto_detect=1
# Enable DRM VC4 V3D driver
dtoverlay=vc4-kms-v3d
max_framebuffers=2
# Run in 64-bit mode
arm_64bit=1
# Disable compensation for displays with overscan
disable_overscan=1
[cm4]
# Enable host mode on the 2711 built-in XHCI USB controller.
# This line should be removed if the legacy DWC2 controller is required
# (e.g. for USB device mode) or if USB support is not required.
otg_mode=1
[all]
[pi4]
# Run as fast as firmware / board allows
arm_boost=1
[all]
enable_uart=1
dtoverlay=dwc2,dr_mode=host
dtparam=ant2
disable_splash=1
ignore_lcd=1
dtoverlay=vc4-kms-v3d-pi4
dtoverlay=i2c3,pins_4_5
gpio=13=pu
dtoverlay=reTerminal-bridge
dtoverlay=reTerminal,tp_rotate=1
dtoverlay=reTerminal,addr=0x20,mcp23008