ReSpeaker XVF3800 hangs after computer reboot

On a booted Linux system, I plug in my new ReSpeaker XVF3800 to USB and it works fine.

After rebooting the host computer (soft reboot, not power cycle), the ReSpeaker no longer works. Simple system tools like arecord return errors trying to access the device.

Pressing the reset button on the side of the ReSpeaker restores it to operation. So, of course, does physically unplugging the USB cable and plugging it back it.

I’ve tried resetting the device with usbreset (Linux command). No luck. It seems that the ReSpeaker is getting into a bad state after any reboot that requires it to be hard reset in order to restore it to operation.

I am on firmware 2.0.7. I’ve tested this on multiple host computers. It makes the device pretty useless since it cannot survive computer reboot without manual intervention (unplug/replug or reset button).

Any suggestions?

Hi there,

So, If I were a gambler my money is on a “firmware BUG” something related to the USB power state. It’s NOT a Linux or Host issue, your results prove it. :face_with_peeking_eye:
The behavior you describe is classic:

  • Works after cold power-up
  • Fails after host reboot (warm reset)
  • Recovers only after device reset or full USB power removal

That means the device does not correctly re-initialize its USB stack when VBUS never drops.

Linux reboot ≠ USB power cycle.
usbreset does nothing (it resets the host port, not the device MCU/DSP)
usbreset:

  • Sends a USB port reset
  • Does not reset:
    • Device MCU
    • DSP core
    • Internal USB audio state machines

If the firmware is wedged internally, the host cannot fix it.
try a USB hub that is powered with a switch , try that (temp)
Even a cheap hub sometimes works because many hubs do cut VBUS on reset.
You can check the BIOS/UEFI boot options too, but I’m money on BUG in firmware..
ok, to look anyway, Turn off any “Always ON USB” options.

The fact that the reset button works instantly proves:

  • Firmware reset path is fine
  • USB reset path is incomplete

This is firmware defect territory.

AI, agrees and points out the specific steps of possible failures.

One or more of these is almost certainly true:

  1. No proper USB bus reset handler
  2. DSP not restarted on USB reset
  3. Clock domain not reinitialized
  4. USB Audio Class endpoints not re-armed
  5. Power management bug (suspend/resume mishandled)

This is very common in:

  • Audio DSP devices
  • Voice front-end chips
  • USB composite devices with internal RTOS

HTH
GL :slight_smile: PJ :v:

Send an E-mail to support,
You should explicitly ask:

Does the XVF3800 firmware correctly handle USB bus reset without VBUS removal?

And request:

  • Firmware with full USB reset handling

:+1:

PJ_Glasso: thanks for your response. I think you are right it is a firmware issue but I was hoping someone could suggest a software workaround to force a reset on the ReSpeaker without dropping power. I will follow up with an email to the Seeedstudio email tech support address but my last query to that address (concerning a bricked XVF3000 based V2 ReSpeaker) has been unanswered for a week … so far.

If anyone can confirm that they also see this behavior where the XVF3800 USB ReSpeaker cannot survive a warm boot, that would be helpful. Surely I’m not the only person this is affecting!

Hi there,

No worries,
I agree 100%, also it’s the USB reset there’s the conundrum, It won’t reset unless it’s repowered, so no Host side USBreset (normally it would) or INIT will get it done.
Keep it going they will get to us asap I’m certain. :lying_face:
:grin:

it’s a brand new product so some bumps are expected, but the lineage is long for this family so , IMO I think they have very good handle on the hardware, just tuning up the firmware side it lagging. they will get there.:crossed_fingers:

HTH
GL :slight_smile: PJ :v:

Hello there, i have the exactly same error also,have you find solution?i tried also to downgrade and the same issue.I use it to a robot so when it turn on i have to unplug the usb and set it back but this is not that helpfull at all for me .

I have worked with Seeedstudio tech support extensively on this. They say they have reproduced the problem, but so far they have not fixed it weeks later. I will send them another message soon to check on status. The problem does not appear in Windows on some machines I have tested on. It also does not appear on some laptops that I test on (possibly those machines do a different USB reset on softboot).

For me coming when I start up the raspberry from the button also when I did fresh start unplugged and plug in the power again.i want to see if I can reset it before I start the script of the robot

Hi there,

Yes , the reseting was a problem. but only in certain Scenarios AFAIK
Reset it before may be the work_around in the startup/. :v: even on the older unit this was a thing. Powering it on Last was the work_around_ fix then too, If I recall correctly.

GL :slight_smile: PJ :v:

Finally I got a workaround from Seeedstudio tech support! Get the xvh_host.py tool from here:

https://github.com/respeaker/reSpeaker_XVF3800_USB_4MIC_ARRAY/blob/master/python_control/xvf_host.py

You will need the pyusb library and its dependencies (install via pip or uv recommended).

In your system startup you reset the reSpeaker by running something like:

xvf_host.py REBOOT –values 1

Then you can soft reboot the computer and the reSpeaker will continue to work.

thank you for that finally i can run it before my code but for my rpi5 i have to uncomment the #import libusb_package to work because coming error import libusb_package
ModuleNotFoundError: No module named ‘libusb_package’