ReSpeaker Mic Array v2.0 Pinout J5/6

Hello!
Can you provide some additional information on the connectors J5/6? I looks like USB is available on the Pins but how about Audio out (instead of the 3.5 connector).

Best regards

Volker

Hi Volker,


please refer to below picture.



Thanks

best rgds
Bill

Hello Bill,

thank you for your feedback. I found this picture already on the web.
But what is HP_L or HP_R? What is “Speaker”?

Where do I find the additional 6 pins in the bottom right? Are these the
pads from the 3.5mm Audio jack?

What about the connectors at the back? Are they the same pin out as the
top pads?
Best regards

Volker

Hi

Volker


1. But what is HP_L or HP_R? What is "Speaker"?

It is headphone left and right.

2. Where do I find the additional 6 pins in the bottom right? Are these the pads from the 3.5mm Audio jack?

You can not find it on the bottom side, the pads on bottom side are not 3.5mm audio jack.

pin2/6/1/5 are connected to gnd, 7&3 and 4&8 are connected together. you only need to care about the hp_l and hp_r, GND as well.


3. What about the connectors at the back? Are they the same pin out as the top pads?

we updated the product and remove the pin connectors at back side, only leave the pads and the bottom pins are the same as top pins.

Thanks

best rgds
Bill

Hello Bill,

thank you for your updates. This is now more clear to me!

One file question: where do I find these pins (see attached file). And
what is “Speaker” and “USB”?
Regards

Volker

Hi

Volker


Please see below picture.



Thanks

best rgds
Bill