ReSpeaker Mic Array v2.0 - Not able to update firmware from Windows 10 using dfu_windows.py

Hello,

I am not able to update ReSpeaker Mic Array v2.0 firmware from Windows 10 using dfu_windows.py.

Getting below error as No re-enumerated DFU device found. Can someone help on this issue.

entering dfu mode
Traceback (most recent call last):
File “C:\Users\SANATH DEEPA\usb_4_mic_array\dfu_windows.py”, line 235, in
main()
File “C:\Users\SANATH DEEPA\AppData\Local\Programs\Python\Python310\lib\site-packages\click\core.py”, line 1130, in call
return self.main(*args, **kwargs)
File “C:\Users\SANATH DEEPA\AppData\Local\Programs\Python\Python310\lib\site-packages\click\core.py”, line 1055, in main
rv = self.invoke(ctx)
File “C:\Users\SANATH DEEPA\AppData\Local\Programs\Python\Python310\lib\site-packages\click\core.py”, line 1404, in invoke
return ctx.invoke(self.callback, **ctx.params)
File “C:\Users\SANATH DEEPA\AppData\Local\Programs\Python\Python310\lib\site-packages\click\core.py”, line 760, in invoke
return __callback(*args, **kwargs)
File “C:\Users\SANATH DEEPA\usb_4_mic_array\dfu_windows.py”, line 226, in main
with dev:
File “C:\Users\SANATH DEEPA\usb_4_mic_array\dfu_windows.py”, line 108, in enter
raise ValueError(‘No re-enumerated DFU device found’)
ValueError: No re-enumerated DFU device found