ReSpeaker Mic Array v2.0 as PC mic input & audio output

I work on databases and i have no experience in this field, but , for a new project this board seems a good choice.
My question is, when connected to Windows PC via USB, can this board work as mic input on pc and audio output?
The desired result is to have the PC audio output on Matrix board audio jack and the board to be seen on PC as a microphone (to set it as default communication device). Is it possible?

Yes, It’s possible and it’s a plug and play USB device.

Thank you evry much.
Any source to buy it from Europe?

is ReSpeaker-Core-Based-On-MT7688-and-OpenWRT necessary or buying only ReSpeaker Mic Array v2.0 enough for my project? As i wrote i only want it to act as mic input on pc and audio output from pc

ReSpeaker Mic Array v2.0 would be good.
The MT7688 ReSpeaker Core has been End-of-Life.

can a display be connected on Respeaker Core V2 by some way?

A monitor can connected to the board via HDMI port. Are you talking about a mini LCD display?

yes, mini touch (capacitive) LCD module. i think i would have difficulty to make the touch function work