ReSpeaker Lite - USB 2-Mic Array Studio XIAO ESP32S3 (Sense)

ReSpeaker Lite - USB 2-Mic Array Studio XIAO ESP32S3 (Sense)

I have tested all examples but I cant get any sound out , also I don’t understand how to upgrade the firm ware.

Do any one have experience of this ?

Would be so happy to get help

Hi there,
Yea, one thread is sufficient when seeking help. What have you tried.
You can delete the other thread and keep all the info in one spot for others to find as well.
which firmware from where?
Have you read the wiki , what part doesn’t work?
It’s the S3 which BSP are you using? can you roll it back and try an older Board Support package(boards tab) arduino IDE.
HTH
GL :slight_smile: PJ :v:

you have a picture of how it is connected?

Sorry PJ

First time here, I will be better in the future

Hi there,
No worries, it is to benefit everyone. So It sounds like you compiled and flashed the device yes or no?
you can try first the BSP (boards Support package) espprssif updated there stufff and a lot of older demo won’t run with the newer BSP. in the boards tab in Arduino IDE You can pick the version. I would roll back to 2.0.17 or 3.0.0 and try with those.
You using head phones?
HTH
GL :slight_smile: PJ :v:

Thanks!!!
Yes using headphones
I just got the Respeaker board it should have the latest firmware