ReSpeaker 6-Mic Circular Array Kit for Raspberry Pi & TDM output

Hi
I want to connect this Raspberry Pi with two Evaluation Module(TAS6424-Q1)
like this
Seed 6-mic analogout -> TDM digital out-> Left channel(TAS6424-Q1) + Right channel(TAS6424-Q1)

so,what do I need or what should I do
if I want to convert the output of this Raspberry Pi into TDM digital out

ReSpeaker 6-mic Circular Array Kit above is a PCM signal that is not a TDM signal.

Thank you for the information
and,Is there any additional equipment for signal conversion for this Raspberry Pi ?

ReSpeaker 4-Mic Array for Raspberry Pi can output TDM signal,
and ReSpeaker 6-mic Circular Array Kit have same IC(AC108),
so,is there any way to let ReSpeaker 6-mic Circular Array Kit can output TDM signal.