Hello,
I want to use the Respeaker 4-mic array with a jetson nano but I have the following queries:
- The 2mic hat has a driver to run with jetson nano. Is there a driver for the 4 mic array and jetson nano?
- I have other sensors interfaced with the nano as well so I do not want to dedicate the complete 40 pin GPIO to the array. Which connections or pins are essential for the complete array to work. From the FAQ I see I2S is needed for sound, I2c for control data and SPI for led control. I am assuming we need to more pins for power and ground. Are there any other pins we need or can we just use these pins to achieve all functionality
- does the Respeaker 4 allow for direction of arrival detection?
Thank you