Hi,
I’m using a ReSpeaker 2-Mics Pi HAT on a Pi zero W. The on-board PA102 LEDs are randomly switched on at startup and stay on. Sometimes its only one LED sometimes it’s all three of them. Is there a way to configure them so that they are all switched OFF at startup?
Thanks in advance…
Eric
Hi there:
You can change to </s>def write(self, colors):
for i in range(self.PIXELS_N):
self.dev.set_pixel(i, int(colors[3*i]), int(colors[3*i + 1]), int(colors[3*i + 2]))<e></s>def write(self, colors):
#for i in range(self.PIXELS_N):
#self.dev.set_pixel(i, int(colors[3*i]), int(colors[3*i + 1]), int(colors[3*i + 2]))<e>