Reset reTerminal E1001 to pair with another account

Hi, I am using the “E1001” and have deleted it from my account. I am planning to pair it with another account at “sensecraft.seeed.cc/hmi,” but the PIN is not showing up, even after updating the firmware in factory reset mode. The user interface is stuck on the default page, even after connecting to Wi-Fi.

Thanks in advance.

Hi there,

and Welcome Back…

so, Yes, there are documented troubleshooting steps to resolve this. When a reTerminal E1001 is deleted from a SenseCraft account, the device itself doesn’t automatically know it has been unlinked. It remains trapped in its old state, which prevents it from generating a new pairing PIN even if you flash the firmware.

To fix this and force the device to generate a new pairing code, try the following sequence:

1. Hard-Reset the Wi-Fi Profile

If the user interface is stuck on the default home page, it is likely still trying to use old handshake data. You need to wipe the network configuration to trigger a clean boot cycle.

  • On the device: Press and hold both navigation buttons (left and right) simultaneously for 2 seconds .
  • This will force the reTerminal to drop its current network attachment and return to its initial provisioning state.

2. Re-Provision via the Access Point

Instead of relying on the web dashboard right away, go through the local AP setup to ensure a clean binding code is generated:

  1. Connect your smartphone or computer to the local Wi-Fi hotspot broadcast by the device. The network name will look like reTerminal E1001-{MAC Address} (no password required).
  2. If the configuration portal doesn’t pop up automatically, open a web browser and go to 192.168.4.1.
  3. Re-enter your 2.4 GHz Wi-Fi credentials and hit Save.
  4. Once the device reconnects successfully, it should emit a confirmation beep and refresh the e-ink screen to display a new pairing PIN.

3. If it remains stuck (Alternative Flash Method)

If standard factory flashing via the SenseCraft HMI flasher keeps resulting in a frozen screen, the background pairing flags may be corrupted in the ESP32-S3’s non-volatile storage (NVS).

You can clear the internal memory completely by navigating to the TRMNL Web Flasher, plugging the device into your PC via USB-C, and executing a Full Flash (Erase All) using their public firmware. Once completely wiped, you can cleanly switch it back to the official SenseCraft HMI firmware via the SenseCraft device utility page, which will guarantee the device boots up completely empty and generates a fresh setup code.

HTH
GL :slight_smile: PJ :v:

Hi @PJ_Glasso , Thanks for the response. I tried all of these, even erased the flash with espweb too, and flashed back to HMI firmware, but still no pairing PIN is shown.

Hi there,

No worries, the last one is what should work. Something else maybe’s afoot?
What mobile device you using , may I know ?

Is it doa looking or are there any signs of it alive after the last factory flashing ?
I will look into it further.

Hang in there.

GL :slight_smile: PJ :v:

After the reset, it’s properly connected to the internet, and I also checked the local page on the computer, so it’s not about the mobile.

I can see the reflashing is successful

@PJ_Glasso You appear to be the guru on this issue, do you have any suggestions for me?

I am also having this same problem, but with a reTerminal E1002. I have flashed the firmware to TRMNL, Arduino, and ESPHome, each time with a “full” erase and re-flash via (I can’t include links in my posts, so here is an approxomation of the URL)
seeed-projectsgithubio/OSHW-reTerminal-Series-E-D/

After the firmware has flashed, I then go to:
sensecraftseeedcc/hmi/tools/firmware

…to complete the firmware erase and re-flash so I can use my e1002 with Sensecraft Seeedash. The problem is that after the re-flash, once I connect my device to WiFi, it is registered to another user’s account. As soon as it joins the WiFi, then it downloads the other users current/last project and displays it. At no point, once I have connected the e1002 to WiFi, do I get a pairing PIN code.

Is there any way to remove my device from another user’s account?

FYI: Why? My e1002 was purchased from Amazon as a returned device. Yes, I can return it to Amazon identifying it as defective, but I figure there must be a way around this issue. I don’t want to see this e1002 go to e-waste just because it was paired to another user’s account.

Hi there,

SO , it appears its the cloud issue and not being unbound…

Why flashing doesn’t clear the pairing

The binding between the reTerminal (E1001 / E1002) and a Seeedash/SenseCraft account lives in the cloud on Seeed’s backend servers, not in local ESP32 flash memory:

  • When the reTerminal boots official firmware and connects to Wi-Fi, it reports its unique hardware identifier (factory MAC address / Chip ID) to Seeed’s SenseCraft backend.

  • If that hardware ID is still registered to the previous owner’s account in Seeed’s database, the server automatically associates it and pushes down the previous owner’s dashboard project.

  • A local flash erase (esptool.py erase_flash) wipes the local NVS, Wi-Fi credentials, and code, but as soon as you re-flash the official firmware and reconnect to the internet, the backend instantly recognizes the MAC address again.

How to resolve it

  • Official SenseCraft / Seeedash unbinding: The user needs to contact Seeed Studio support or forum staff (@Seeed_John / technical support) with the device’s MAC address and Serial Number / Proof of Purchase. Seeed support must manually unbind or release the hardware ID from their backend database.

  • Alternative open-source route (Bypass SenseCraft): If they don’t want to wait for Seeed backend support, they can use standalone third-party firmwares that do not touch Seeed’s cloud (e.g., custom ESPHome, TRMNL, or Home Assistant e-paper dashboards pointing to a local Home Assistant instance or independent server).

Send pictures of the unit as well. :+1:

HTH
GL :slight_smile: PJ :v:

Thank you, that makes sense and what I figured the problem was, but I didn’t know who/how to fix it.

I’m new to this forum, so I’ll have to figure out if there is a PM system so I don’t post my MAC/serial no/proof of purchase for everyone to see.

Thanks again!

I was able to fix it by contacting the Seeed team (Thanks for Meililly) and remove the already paired account.

So what happened is, I used this device for a e-ink workshop and on of the participants is paired with this device as part of the workshop and did experiment, and at the end I asked everyone to un-pair and all confirmed they did, but unfortunately they didn’t done that even I asked to check again and there is no way to find that.

So after many day and multiple tries, with seeed team, was able to fix it be removing that account.

Hi there,

Glad you got it sorted out… I hope the info was helpful
and thanks for letting us know it was resolved.

GL :slight_smile: PJ :v: