reServer AI NVR - Jetson Orin NX 16GB, Jetpack 6.2.1 SATA Devices not recognised

After updating to Jetpack 6.2.1, my SATA SSD has stopped showing up.
There is no sda device in lsblk output, and I can’t see the SATA bridge in lspci output either.

Has anyone seen this before / know how to solve the issue?

Hi there,

So, It’s not Normal but updating often can have this arise if the Seeed builds DeviceTree isn’t included or if the hardware, like the sata controller or driver changes.
I pretty sure that is why the Vanilla Nvidia’s “upgrade” doesn’t work on most clones.
also why the wiki advises using a ubuntu host for the build or update (the generic DT) just works.
Since the platform is Seeed Studio reServer AI NVR (Jetson Orin NX 16GB), the SATA drives in that system are not native SATA from the SoC. They are exposed through a PCIe-to-SATA bridge on the carrier board. So the storage chain looks like this:

Jetson Orin NX
     │
     └─ PCIe root port
           │
           └─ PCIe → SATA bridge chip
                 │
                 └─ SATA drives (sda, sdb, etc.)

If the bridge disappears from lspci, the problem is before Linux storage drivers — it means the PCIe device is not being enumerated.

On Jetson systems this almost always comes down to one of three things after a JetPack upgrade.

:one: Carrier-board Device Tree got replaced

JetPack updates frequently install a new kernel + default NVIDIA DTB.

The NVIDIA JetPack update can overwrite the carrier-board specific device tree that enables:

  • PCIe lanes
  • PCIe reset GPIOs
  • slot power rails
  • bridge devices

The NVIDIA Jetson Orin NX dev kit DTB does not contain the hardware definitions for the reServer carrier board, so if that DTB gets used instead, the PCIe bridge powering the SATA controller never comes up.

Result:

lspci → bridge missing
lsblk → no drives

:two: BSP / overlay package not reinstalled

Seeed’s Jetson systems usually ship with a custom BSP layer that includes:

  • carrier-board DT overlays
  • PCIe configuration
  • GPIO power enable
  • fan + LED controls

After upgrading to JetPack 6.2.1, the system may now be running the generic NVIDIA kernel + DTB, not the Seeed BSP.

Reinstalling the board support package normally fixes it.

:three: PCIe power-enable GPIO not configured

Some carriers use a GPIO to power the SATA bridge chip.
If that GPIO is not configured by the DT anymore, the bridge simply never powers on.
Linux then behaves exactly like you described.

Check which device tree is loaded:
cat /proc/device-tree/model

If this is a reServer system, the model should reference the reServer carrier board, not just the Jetson module.

If the wrong DTB is being used, reinstalling the Seeed BSP / device-tree overlays for JetPack 6.2.1 should restore the PCIe bridge and the SATA devices. :+1:

HTH
GL :slight_smile: PJ :v:

seed1@seed1-desktop:~$ cat /proc/device-tree/model
NVIDIA Jetson Orin NX Engineering Reference Developer Kit Superseed1@seed1-desktop:~$ 

So it seems the Seeed BSP is not being used, however I followed Seeed’s flashing instructions and used the image from Seeed’s site….

That’s a tricky one when the SATA bridge disappears from lspci, it usually points to a driver or firmware issue after the Jetpack update rather than just a disk detection problem. I’d double-check the board-specific drivers and any kernel modules tied to SATA support, since updates in Jetpack 6.x sometimes change hardware support layers. Tools like X111 also show how stable system compatibility is crucial, especially when dealing with hardware-dependent setups like this.