Hi, I didn’t received any answer regrading this issue.
Can I record in higher rate than 16kHz in the ReSpeaker Mic Array v2.0?
In your site you say the max rate is 48kHz but python send an error “OSError: [Errno -9997] Invalid sample rate” for the following rates: 44000, 44100, 48000.
So, what is the max record sample rate that I can record at, and what is the parameter I need to enter in order to record in that max sample rate.
best regards
davidpodless