How do I record an image with recamera at full resolution, 2592 x 1944 @ ~ 1fps? The NodeRed camera max resolution (dropdown) is only 1920 x 1080.
Ultimately I would like to create an https endpoint to grab the current image and run the image itself through a custom cnn.