Hi, I have recently bought an Re-speaker Mic array v2.0 and installed 6-channel firmware. I would like to know how to record each channel separately(Especially channel0 which has processed audio for ASR). A python implementation would be great!!
Hi there,
here is the python example, <LINK_TEXT text=“http://wiki.seeedstudio.com/ReSpeaker_M … ract-voice”>http://wiki.seeedstudio.com/ReSpeaker_Mic_Array_v2.0/#extract-voice</LINK_TEXT> thanks.
Thanks for your reply. I already went through that link but didn’t help my scenario. But I was finally able to solve my issue 
hi
how to record channel seperately? the python example only show record all channels
Hi there,
Here is the code and configure the channel. thanks.
# deinterleave, select 1 channel
channel0 = data_array[0:]
#channel1 = data_array[1:]
# convert numpy array to string
data = channel0.tostring()
frames.append(data)
[code]import sys
import pyaudio
import wave
import numpy as np
CHUNK = 1024
FORMAT = pyaudio.paInt16
CHANNELS = 6
RATE = 16000
RECORD_SECONDS = 5
pyaudio_instance = pyaudio.PyAudio()
find the index of respeaker usb device
def find_device_index():
found = -1
for i in range(pyaudio_instance.get_device_count()):
dev = pyaudio_instance.get_device_info_by_index(i)
name = dev['name'].encode('utf-8')
print(i, name, dev['maxInputChannels'], dev['maxOutputChannels'])
if name.lower().find(b'respeaker') >= 0 and dev['maxInputChannels'] > 0:
found = i
break
return found
device_index = find_device_index()
if device_index < 0:
print(‘No ReSpeaker USB device found’)
sys.exit(1)
stream = pyaudio_instance.open(format=FORMAT,
channels=CHANNELS,
rate=RATE,
input=True,
input_device_index=device_index,
frames_per_buffer=CHUNK)
print("* recording")
frames = []
for i in range(0, int(RATE / CHUNK * RECORD_SECONDS)):
data = stream.read(CHUNK)
# convert string to numpy array
data_array = np.fromstring(data, dtype='int16')
# deinterleave, select 1 channel
channel0 = data_array[0:]
#channel1 = data_array[1:]
# convert numpy array to string
data = channel0.tostring()
frames.append(data)
print("* done recording")
stream.stop_stream()
stream.close()
pyaudio_instance.terminate()
wf = wave.open(‘out.wav’, ‘wb’)
wf.setnchannels(1)
wf.setsampwidth(pyaudio_instance.get_sample_size(FORMAT))
wf.setframerate(RATE)
wf.writeframes(b’’.join(frames))
wf.close()[/code]