reComputer Super J4012 AX210.NGW Wi-Fi Card Not Working After Updating to JetPack 7.2

原本在reComputer Super J4012中系統是JETAPCK6.2 可以正常使用AX210.NGW 無線網卡 不用安裝任何驅動

根據WIKI更新到JETAPCK7.2 之後無法使用AX210.NGW 無線網卡 有嘗試過安裝相關套件但還是無法使用
請問有建議的套件更新嗎?
還是有其他建議J4012 在JETAPCK7.2 可以使用的無線網卡嗎?

The reComputer Super J4012 was originally running JetPack 6.2, and the Intel AX210.NGW wireless network card worked properly without installing any additional drivers.

After upgrading the system to JetPack 7.2, the AX210.NGW wireless card is no longer detected or functioning.

I have already tried installing several related packages and drivers, but the wireless card still does not work.

Could you please advise:

  1. Are there any recommended packages, drivers, or firmware updates for using the Intel AX210.NGW on JetPack 7.2?

  2. Is the Intel AX210.NGW currently supported on JetPack 7.2?

  3. If not, could you recommend a Wi-Fi adapter that is fully compatible with the reComputer Super J4012 running JetPack 7.2?

Any suggestions or guidance would be greatly appreciated.

Hi,

We confirm the issue you reported exists. Please download the drivers from the two links below and replace the corresponding files at the following paths:

/lib/modules/$(uname -r)/kernel/drivers/net/wireless/intel/iwlwifi/iwlwifi.ko

/lib/modules/$(uname -r)/kernel/drivers/net/wireless/intel/iwlwifi/mvm/iwlmvm.ko

After replacement, run the command sudo depmod -a. Could you check if the Wi-Fi works properly afterwards?

iwlwifi.ko

iwlmvm.ko

Hi there,

Did you get this going ?

GL :slight_smile: PJ :v: