Recomputer R1000 UPS shutdown, no recovery

Hi,

I’ve installed the UPS board on the R1000. Once the power source goes offline, there is a shutdown issued by the OS. The OS will stop all running services and put the CM4 in shutdown. Once the power source is active again, the CM4 will reboot.
However when the powersource comes back online in the middle off the shutdown process, the CM4 will still shutdown and never reboot until the powersource is disconnected and connected again.

Is this a design issue or I’m missing something?

regards,

Kris

Hi there,

I have exactly the same behaviour.

My R1000 is running on balenaOS for CM4 with the documented confix.txt entries and additional:
dtoverlay=gpio-shutdown,gpio_pin=25,active_low=1

The UPS controller LTC3350 should be connected to I2C bus 6 (seeed studio docs) with adress 0x09 (analog device datasheet). I have not found any anvailable kernel module and device tree overlay to communicate with the chip.

I would welcome other solutions or improvements.

Regards,
Hannes

Hi,

I’m using that same entry in the config.txt, and once the power source is gone It’s shutting down the CM4 as described ie: the shutdown command is issued, so no problem there.
A quick Google tells me that there has been a driver for the LTC3350 integrated in the kernel a couple of months ago. [LKML: Sebastian Reichel: Re: [PATCH v5 5/5] power: supply: ltc3350-charger: Add driver](https://LTC3350 kernel driver)
However the schematic of the UPS seems not to be released by SEEED so I cannot make any conclusions or assumptions solely based on the datasheet of the LTC3350.
Also I don’t think the LTC3350 can solve the issue we are having.

Looking at the schematics SEEED released.
The GLOBAL_EN pin of the CM4 has to be pulled down for > 1 ms to restart the PMIC of the CM4. this pin, is controlled by a 74LVC1G34 buffer. This buffer is controlled by the INT pin of the RTC and powered by VDD_5_SYS.
So here is what I think is going on: the INT pin, by default is always high. So basically the GLOBAL_EN will only go low if VDD_5_SYS < 1.65 (see datasheet) for a long enough period. In this case the CM4 will restart automatically if the power source is back online. However if the power is restored if VDD_5_SYS > 1.65V, the output of the buffer will not change, and therefore never trigger a change of the GLOBAL_EN pin.
So maybe there is a way around this? To solve this problem we can activate the Timer of the RTC at shutdown. If the CM4 shuts down, the RTC (powered by the battery) will issue the INT pin if the timer expires and if the power has been restored in the meantime the CM4 will boot up again.
Does this make sense?

regards,

Kris

Hi,
Thanks for your report and further information. Our team will investigate into this issue, and updates will be posted here.

Hi,
Im using this line on config.txt with raspbian
dtoverlay=gpio-shutdown,gpio_pin=25,active_low=1

But when i turn off powersupply, a menu ask me if i want to shutdown or reboot.

Anyone else have this problem? is there a new version of raspbian packaged by seedstudio that fix this issue?

Regards!

Oscar M.

This sounds like an interesting workaround.

Did you have any success in implementing it?

Hi Oscar,

What you’re seeing is normal behavior and not a bug in the Seeed or Raspberry Pi OS image.

The overlay:

dtoverlay=gpio-shutdown,gpio_pin=25,active_low=1

doesn’t force the Pi to shutdown automatically.
It simply generates a power-button event at the OS level.

On Raspberry Pi OS with the desktop running, a power-button event triggers the Shutdown / Reboot / Cancel menu. That’s why the confirmation dialog appears when you turn off the power supply — the OS is just reacting like a regular PC power button.

Nothing is wrong with the overlay, and there isn’t a newer Seeed release that “fixes” this because the behavior is intentional.

If you want the button to shut down instantly (no menu)

There’s no config.txt switch that automatically confirms the dialog.
But you can bypass the GUI dialog entirely with one of these methods:

Option 1 — Run the Pi without the GUI (Lite / headless)

On a headless system, the same overlay usually results in an immediate shutdown.

Option 2 — Handle the GPIO yourself in a script

Instead of relying on gpio-shutdown, you can read GPIO 25 in a small script and call shutdown directly:

from gpiozero import Button
from signal import pause
import os

power_button = Button(25, pull_up=True)

def handle_press():
    os.system("sudo shutdown -h now")

power_button.when_pressed = handle_press
pause()

Run that on boot (via systemd), and remove the gpio-shutdown overlay.
Then a power-button press will perform an immediate, no-questions-asked shutdown.

HTH

GL :slight_smile: PJ :v:

Any update on this? I have the same issue, if the power returns before the UPS supercap is depleted, the device never powers up again.

I ended up coding a I2C driver in Python for both health and backup status monitoring of the SuperCAP cross referenced against the published LTC3350 datasheet and SuperCAP schematic.

For shutdown I monitor the discharge state of the UPS and make a last second decision to sync and shutdown instead of shutting down straight away. This way quick power outages are handled (knocking a cable out on my workbench) and the time between shutdown and SuperCap discharge is reduced to a few seconds, meaning the condition preventing CM4 power up is minimised.

Also added in health monitoring of the Super Caps and module overall to monitor for age degradation.

I’ve cleaned it up and put it onto github .com/lucasnetau/ltc33500-ups (forum preventing me from publishing links)