reComputer Jetson-10

Hi

Currently my host computer Ubuntu version is 20.04 I need to flash jetpack 4.3 version to the recomputer jetson 10-1-H0 carrier board the default version in the board is 4.6. I tried flashing using command line mode. But the cuda , cudnn and tensorrt was not installed default after the jetpack installation. Can you provide me the solution to flash the board with installing all these jetpack packages during flasing itself. O

Thanks in advance

Hi,Gayathri:
First, we should check if our reComputer Jetson module supports the Jetson Linux version.In addition, may I ask what kind of product you have? J1010 or ohter?

what do you mean by jetson linux version. When i try to flash the device through command line , the cuda , cudnn and tensorrt was not installed by default.